AXIS#.HOME.PERRTHRESH

Description

AXIS#.HOME.PERRTHRES is the maximum value the absolute following error (AXIS#.PL.ERR ) needs to exceed to detect a mechanical stop.

AXIS#.HOME.PERRTHRES is only used when homing against a mechanical stop using AXIS#.HOME.MODE is 8, 9 or 10.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

180 deg

Data Type

Float

See Also

AXIS#.HOME.IPEAK
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
AXIS1.HOME.PERRTHRESH

5008h

06h

Signed32

Position

-

Read/Write

No

AXIS2.HOME.PERRTHRESH

5108h

06h

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.PERRTHRESH

6110

17DE

Signed32

Read/Write

Position

AXIS2.HOME.PERRTHRESH

71646

117D

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.PERRTHRESH

6110

Signed32

Read/Write

Position

Related Topics

Homing